This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430FR5969: MSP430 compiler issue

Part Number: MSP430FR5969

Tool/software: Code Composer Studio

Hi,

My customer reported unexpected compile results for MSP430FR5969.

TI compiler version: 20.2.2.LTS and 18.12.6.LTS are tested and results were the same.
Optimization level: “4 - Whole Program Optimizetions”

Below C sources are compiled to each asm code.

a)
SystemParameters.AlarmToneVolume.Data = SystemParamDefault.AlarmToneVolume.Data;
=>
1840 4292 AE9E 446A   MOVX.W &0x0ae9e,&0x0446a

b)
SystemParameters.BatteryVoltageLevel.Kind = SystemParamDefault.BatteryVoltageLevel.Kind;
=>
40B2 3331 4444       MOV.W   #0x3331,&0x4444

c)
SystemParameters.TimeOutSetting.Data.DoseDispTime = SystemParamDefault.TimeOutSetting.Data.DoseDispTime;
=>
1840 42D2 AE50 441C   MOVX.B &0x0ae50,&0x0441c

Customer expects the b) should be complied to;
MOV.W &0x0ae78,&0x4444
where “&0x0ae78” is an address of SystemParamDefault.BatteryVoltageLevel.Kind
But immediate value “#0x3331” is used instead.

If the optimization level is changed to “3 - Interprocedure Optimizations”, the issue is gone.
But in this case, performance is not enough to meet their system requirements.

Thanks and regards,
Koichiro Tashiro