This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: unable to remove single include path

Tool/software: Code Composer Studio

short description: I am unable to remove a single entry from my include path list. This is not the behavior I would expect and I think it could possibly be a bug.

In the project properties under CCS build > Include Options, there is a dialog with the header "Add dir to #include search path (--include_path, l)".

It contains a list of the paths that are configured as include paths. On the upper right corner of that dialog there are a few control buttons, one of them is "delete".

I have several include path entries listed in this dialog and I want to remove one of them. My problem is that no matter how I try, clicking the mentioned delete button removes all entries in my list.

The same behaviour is found for other "path dialogs", for instance

CCS Build > ARM Linker > File Search Path (there are two here)

CCS Build > ARM Linker > Advanced Options > Command File Preprocessing

CCS Build > ARM Linker > Advanced Options > Linker Output

CCS Build > ARM Linker > Advanced Options > Miscellaneous

(my list may not be exhaustive, there may be other places that I haven't checked)

I expect that marking a single entry and clicking delete should only remove the currently highlighted entry.

If I want to delete more than one entry, I will select several entries and click delete thus removing all marked entries.

A workaround is of course to completely clear the list, and then add only the entries that I need. This is cumbersome and likely not the intended behavior.

I am running Code Composer Studio 10 on a Ubuntu 20 host.