Tool/software: TI C/C++ Compiler
Hi
I have hard time forming a complete picture where we should go with our project.
We are at a decision time and we need to decide on the MCU and SDK.
Yesterday it was all clear that we would go forward with F280049C, DRV8323 and Motorware.
But today after (too much) reading of forums and stuff I'm second guessing this.
Here are some of my concerns
1) Is Motorware a dead end in the long run and we had better switch to C2000WARE-MOTORCONTROL-SDK (if that is the SDK)
or am I mixing things
2) I did not find a ready to run code example for F280049C,+DRV8323 or DRV8305 (which we use atm with F28027 Launchpad),
neither in C2000WARE or Motorware, perhaps I did not look hard enough?
3) We have a motor that should be run at +70 krmp but with Motorware labs I've not been able to get past 32 krpm and
I've not been able to find what is the limiting factor, is it InstaSpin-FOC, MCU or what, are those limits explained somewhere?
4) We have been approaching this with InstaSpin FOC, but is that the right approach? Years ago we experimented in an other project
with Instaspin BLDC but is that still a thing? And would it be a better match for just running the motor at 5-70 krpm speeds, I don't
know if we need or would benefit from the FOC.
All this insecurity came from a simple need to switch evakit to get more memory and changing the motor type and suddenly
everything is up in the air.
Any guidance would be much appreciated!
wbr Kusti