This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TIDA-01580: TIDA-01580 Software

Part Number: TIDA-01580

Tool/software: Code Composer Studio

 I use Mercurial and TortoiseHg as the source control software.

 I can't   write   .hgignore   file.

Please tell me which directories and which files do not need to be saved.

Code Composer Studio       Version: 7.4.0.00015

Unfortunately, there is clearly not enough information.
And the links seem to be outdated.
There are a lot of file extensions used in my project
as well as many directories.
What should be put under version control?

Thanks in advance,