This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CODECOMPOSER: Missing Splitters

Part Number: CODECOMPOSER
Other Parts Discussed in Thread: SYSCONFIG

Tool/software: Code Composer Studio

Hello,

I'm not very used to Eclipse / CCS, but the missing splitters between windows under macOS confuses me totally. When I try to adjust window sizes within the top level view, the cursor does not changes its shape and it's totally unclear where the point is, where I have to drag to move the border between adjacent windows (which then results in moving windows position, not size / border). When using Xcode for example, the cursor form / shape changes when the cursor is between two windows and where I can start dragging the border between them.

Is this a missing feature in Eclipse, or is this a bug in the current version of CCS / Eclipse (using 10.1.0)?

best regards,

Torsten