Part Number: CC3220SF
Tool/software: TI C/C++ Compiler
Hi, I want to include Windows.h and wincrypt.h, because i'm using mbedtls library for encryption and decryption in that mbedtls using this files.
I add mbedtls .c and .h files in my CCS project i when i try to build it i got errors as below
#error "Platform entropy sources only work on Unix and Windows, see MBEDTLS_NO_PLATFORM_ENTROPY in config.h"
#error "This module only works on Unix and Windows, see MBEDTLS_NET_C in config.h"
#error "This module only works on Unix and Windows, see MBEDTLS_TIMING_C in config.h"
#include <sys/stat.h> cannot open this file
i build the mbedtls in Visual studio, it is working fine , when i added the same files i'm getting errors as above in VS a predefined macro was add in pre-processor _WIN32 if define in pre processor i got error
cannot open this file windows.h
can any one suggest me how to solve this problems