This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28379D: ONCE RUN CPU1 ,TARGET DISCONNECTED

Part Number: TMS320F28379D

Tool/software: Code Composer Studio

C28xx_CPU1: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.2.0.00002) 
C28xx_CPU1: Unable to determine target status after 20 attempts
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting.  There may still be breakpoint op-codes embedded in program memory.  It is recommended that you reset the emulator before you connect and reload your program before you continue debugging不知道什么原因,电源测试都正常
The target can connect normally,it can debug also,when I run CPU2,it is also normal,but once I run CPU1 ,it  disconnected。error information as ollows.