Part Number: SM320VC33-EP
Tool/software: Code Composer Studio
We had an old computer that the HD failed and we are trying to connect with or a Blackhawk usb560M emulator.
I am unable to get a version of Code composer and USB560M driver to install. When we install the version below, the driver installs and the setup accepts it but when CC tries to open it says it is not compatible. I have also tried newer CCSv3.3 as listed on sites as it supports the VC33 processor but the setup will not even allow the usb560M driver for the VC33 part. Any suggestions?
code composer CC'c3x-'c4x
COMPONENT VERSION COMPANY
----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Integrated Development Environment 4.10.36 Texas Instruments
Board Revision 00.00.00
Target Silicon Revision 00.00.00
Device Driver Revision 00.00.00
Code Compers Studio Setup
Version 4.10
Build 36
BlackHawk
USB560M Emulator
HW rev 03-6512-1140-C822, SPI24
FW rev 3.02 (R2), Nov 18 2011 11:30:32