Part Number: AMIC110
Tool/software: Code Composer Studio
Hi,
I am using AMIC110, and configured it as EtherCat slave with full slave stack from Bechoff..
While using the code, the project is working when i am debugging the code, But when I flash the same binary file generated in debug mode in to the microcontroller its not working.
I am using "spi_flash_writer_AM335X" to load the binaries.
For flashing the binary I have followed the below steps:
step 1:- flashed boot loader - bootloader_boot_mcspi_a8host_debug_ti.bin (I have choosen this since DDR is enabled) @ Offset: 0x00.
step 2: flashed application (ethercat_slave_full_AMIC11x_arm.bin) @ Offset : 0x20000
Please let me know if any changes to be done in the flashing procedure
kindly provide me a solution for this how to make the code work after flashing also?
Regards,
Hema