Part Number: MSP-EXP430FR5994
Tool/software: Code Composer Studio
I'm having trouble after the initial install of CCS 10.1.0 on my Windows 10 machine. When I try to detect my board, I receive the following error message: {"msg":"COM6: Could not power up the device.","name":"COM6","type":"require-update"}. The board is connected through a USB cable, and LEDs indicate that it is receiving power. On device manager I see two COM ports active when the device is plugged in: MSP Application UART1 (COM5) and MSPDebug Interface(COM6)
Any advice on how to proceed from here?