Tool/software: Code Composer Studio
Hi,
The board I am using is: DB77M24A6426V2
CCS version is: 9.1.0
Industrial Toolbox version is: 3.6.2
on Windows 10.
Question 1:
I burnt the pre-built binaries to the board and then run the Gui on Windows 10. I could see the breath rate and heart rate on the GUI correctly.
but breath rate and heart rate will be wrong if I stand more than around 1m far way from the sensor(board). If I stand within 1m, the rate is correct again.
Is there any way to configure the measurement distance to make it measure more than 1m?
Question 2:
in folder C:\ti\mmwave_industrial_toolbox_3_6_2\labs\lab0026_vital_signs_68xx\gui\profiles, there are 2 configuration files, is there any document that explains all those parameters in those 2 configuration files?
Question 3:
I would like to re-built the source code in folder C:\ti\mmwave_industrial_toolbox_3_6_2\labs\lab0026_vital_signs_68xx\src.
I have CCS and Industrial Toolbox 3.6.2 installed on my computer. If I open CCS, how to create a project for my board?
is there any document that tells me about the method/steps from the beginning?
Thanks and Best Regards,
Ardeal