Other Parts Discussed in Thread: MSP430FR5969
Tool/software: Code Composer Studio
Hi , this is Harikrishna
Currently i am working on Software UART Creation, I successfully created the software UART by using GPIO pin and Bit delay in MSP430FR5969/5994.(We can use Timers for Delay but here i am checking like sending single character from controller Tx)
but i do have some confusion in calculating the delays between bits(bit banging method) to transfer.
i followed the formula like (Clock_Frequency/Baud rate) to maintain delays between successive bits.
ex:
if My clock frequency = 8 Mhz(8000000).
Baud Rate = 9600.
One Bit Delay = 8000000/9600 = 833(working).
I used same number of ( __delay_cycles(800);)delay in my code between two successive bits then my Software UART Transmit(TX) is working and i able to see the information on serial monitor.
One Bit Delay = 8000000/115200 = 69(Not working)
But ,i used the same formula for Different Baud Rate(115200) and its value is 69 is not working and garbage values are printing in serial monitor.
Then after changed manually the value by trail and error method, and UART-TX working with delay value of 21(__delay_cycles(21);) for 115200 Baud Rate.
So literally i confused what really makes the Software UART-TX to work what exactly delay i should Maintain between bits, Because i want to test my Software Uart-Tx with all possible Frequencies that our controller supports.
So please anyone help me that one bit period formula for different frequencies(1Mhz, 2Mhz, 4Mhz, 8Mhz, 16Mhz, 24Mhz, 48Mhz) and different baud rates(9600,,38400,115200). for our Controllers.
Thanks.