Tool/software: Code Composer Studio
Hi all,
I trust you are doing well.
I want help with Audio processing for the multichannel Arm cortex M4 based device.
The process includes
4 channels detecting inputs all the time.
if there is audio coming from any or all ports of the device, the microcontroller should allow the audio coming from ports to be saved in a file on any memory space (Sd card preferred) which can then be played by inbuilt or external DAC by selecting from the menu displayed on LCD attached.
Also, I would mainly need your support only in the Conversion of audio to digital after detecting on ports, the complication for me arrives in multichannel parallel processing of audio, How the sampling must be done?
Also USB intergration.
Also, GSm terminals give gsm line input using a gsm sim card.
I want to which microcontroller I have to choose.
Stay safe
Thanks and regards
Shikhar