This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F5529: Code Composer Studio™ forum

Part Number: MSP430F5529

Tool/software: Code Composer Studio

I am writing a simple bit of code to use assembly to count words and sentences in a string.  I have everything done, and my register counters work like they should.  The problem I am having is that I want to put those counter values into variables "word" and "sent".  I think I have declared the variables correctly, but I cannot find any info on the syntax I need to use to actually put the register count values into the variables I have created.  Is there some syntax for the MOV instruction or maybe ADD instruction I can use to do this?

;code start

        .cdecls C,LIST,"msp430.h"       ; Include device header file

        .def    RESET                   ; Export program entry-point to
                                        ; make it known to linker.

myStr:  .cstring "HELLO WORLD, I AM THE MSP430!"

.data
sent:	.int 0 							; set sentence count variable and initialize to zero
word: 	.int 0 							; set word count variable and initialize to zero

        .text                           ; Assemble into program memory.
        .retain                         ; Override ELF conditional linking
                                        ; and retain current section.
        .retainrefs                     ; And retain any sections that have
                                        ; references to current section.

RESET:  mov.w   #__STACK_END,SP         ; Initialize stack pointer
        mov.w   #WDTPW|WDTHOLD,&WDTCTL  ; Stop watchdog timer

;-------------------------------------------------------------------------------
; Main loop
;-------------------------------------------------------------------------------
main:   bis.b   #0FFh,&P1DIR           	; do not output the result on port pins
        mov.w   #myStr, R4              ; load the starting address of the string into R4
        clr.b   R5                      ; register R5 will serve as a counter for words
        clr.b 	R7						; register R7 will serve as a counter for sentences

gnext:  mov.b   @R4+, R6                ; get a new character
        cmp     #0,R6                   ; is it a null character
        jeq     lend                    ; if yes, go to the end
        cmp.b   #' ',R6                 ; is it a ' ' character
        jne     pun1                   	; if not, go to the next
        inc.w   R5                      ; if yes, increment counter
        mov	R5,&word
        jmp     gnext                   ; go to the next character

pun1:	cmp.b   #'.',R6                 ; is it a null character
        jne     pun2                   	; if not, go to the next
        inc.w   R5                      ; if yes, increment counter
        inc.w	R7						; if yes, increment counter
        jmp     gnext                   ; go to the next character

pun2:	cmp.b   #'?',R6                 ; is it a null character
        jne     pun3                   	; if not, go to the next
        inc.w   R5                      ; if yes, increment counter
        inc.w	R7						; if yes, increment counter
        jmp     gnext                   ; go to the next character

pun3:	cmp.b   #'!',R6                 ; is it a null character
        jne     gnext                   ; if not, go to the next
        inc.w   R5                      ; if yes, increment counter
        inc.w	R7						; if yes, increment counter
        jmp     gnext                   ; go to the next character

lend:   mov.b   R5,&P1OUT               ; write result in P1OUT (not visible on port pins)
        bis.w   #LPM4,SR                ; LPM4
        nop                             ; required only for Debugger

;-------------------------------------------------------------------------------
; Stack Pointer definition
;-------------------------------------------------------------------------------
        .global __STACK_END
        .sect   .stack

;-------------------------------------------------------------------------------
; Interrupt Vectors
;-------------------------------------------------------------------------------
         .sect   ".reset"               ; MSP430 RESET Vector
         .short  RESET
         .end