Part Number: CCSTUDIO
Tool/software: Code Composer Studio
Hi,
I'm attempting to install Code Composer on my Windows Subsystem For Linux, with no success. I'm running Windows 10 Pro, Build 19041.508 with Ubuntu 20.04 via WSL. I've downloaded the CCS 10.1.1 64-bit Linux installer, and to start the installation I run:
./ccs_setup_10.1.1.00004.run --mode unattended --debugtrace /home/jaco/ti.txt --enable-components PF_MSP430,PF_C66AK_KEYSTONE,PF_MMWAVE
The installer quits after a minute or so with no error message or anything (hence the enabling of the debugtrace output). Attached is the ti.txt output file:
/cfs-file/__key/communityserver-discussions-components-files/81/ti.txt
I have the same problem on Ubuntu 18.04 running via WSL.
Regards,
Jaco