Part Number: TMDSEMU110-U
Other Parts Discussed in Thread: AM4377, TMDSIDK437X, AM4379
Tool/software: Code Composer Studio
Hello,
I am having problems getting the xds110 to work correctly with the AM4377. The jtag scan complete with no failures or skips, however when I try using the XDS110 to flash the program onto the board the chip seems to come up badly. Output from the uart shows that the program is getting loaded however parts of the chip dont seem to respond. The internal EEPROM often shows unreadable. Often when this happens the board will partially reset and try booting from sd card or lock up. Debugging has had its own issues as well, please see the mention of that below.
I have asked a previous question (here) about debugging on the AM4377 with the xds110 and I believe they might be related. Unfortunately a bug ticket was made but then closed without a fix.
I have Tried this same thing with a spectrum digital xds200 and had no issues with the exact same target configuration. Is there some other board start up configuration that might be causing me an issue?
Versions:
CCS - 10.1
TI Emulators - 9.2