This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1443BOOST: CCS/IWR1443BOOST

Part Number: IWR1443BOOST

Tool/software: Code Composer Studio

Sir /Mam

As i am working on IWR1443BOOST EVM,in CCS ->Resource explorer, import the high_accuracy_14xx_mss project then build this project, it is generating following errors:

>> Compilation failure
subdir_rules.mk:9: recipe for target 'sensor_mgmt.obj' failed
"..\data_path.h", line 49: fatal error #1965: cannot open source file "ti/demo/io_interface/detected_obj.h"
1 catastrophic error detected in the compilation of "../sensor_mgmt.c".
Compilation terminated.
gmake[1]: *** [sensor_mgmt.obj] Error 1
gmake[1]: Target 'main-build' not remade because of errors.
gmake: *** [all] Error 2
makefile:160: recipe for target 'all' failed

i am unable to resolve the errors .Could you suggest possible solutions.

thanks and regards

Deepshikha