This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler: Can't import project due to missing MSP432 compiler

Tool/software: TI C/C++ Compiler

Hello, I'm trying to import a project from a coworker and am running into this error message:

Import failed for project 'pm-tag-v2' because its compiler definition is not available. Please install the MSP432v20.2 compiler before importing this project:
- See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update.
- Visit CCS App Center to get the latest compiler support.
- Or download and install the compiler [http://software-dl.ti.com/codegen/non-esd/downloads], then register it with CCS through 'Preferences > CCS > Build > Compilers'.

I have tried all 3 of these options and nowhere do I see any compiler with the MSP432 name attached.  I see a lot of stuff about MSP430 compilers but not 432.  I re-ran the CCS installer to confirm I have support for "SimpleLink MSP432 low-power + performance MCUs" installed.  I am running CCS 9.3.  Is there a download link or a way to find this compiler that I'm missing?

Thank you

  • The MSP432 has ARM Cortex-M4F CPU core on it.  So it uses an ARM compiler.  In this case, install ARM Compiler tools version 20.2.x.

    This diagnostic ...

    Erik Simunds1 said:
    Please install the MSP432v20.2 compiler

    ... is confusing.  I'd like to reproduce the behavior and submit a bug report to get it fixed.  You say you imported this project from a co-worker.  Where did they get it from?  

    Thanks and regards,

    -George

  • They created the project as an upgrade from the Version 1 project which used an MSP430.  We upgraded to an MSP432 to use freeRTOS instead of the in-house pseudo-OS that our team created a few years ago.

    I'm not sure all that was involved in getting the project created.  Although I just found out that they said I need the MSP432P4 SDK installed which I don't have, which is probably part of my problem.