Part Number: AWR1443BOOST
Other Parts Discussed in Thread: AWR1443, AWR1642BOOST
Tool/software: Code Composer Studio
Hello,
I have a project running on AWR1443, based on the demo application.
My question is: I would like to use a normal CCS project instead of an RTSC project to avoid having dependencies to some packages installation (SDK, BIOS...). So the other developers will not need to install all the packages again. The goal would be to have one unique folder with all the sources needed to compile the project. I want to avoid problem like : "project not compiling because wrong version of BIOS installed".
Is it possible to do that ?
Thanks