This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMDSDOCK28M36: Problem running the processor M3 of the card F28M36 with CCS

Part Number: TMDSDOCK28M36


Tool/software: Code Composer Studio

Hi Team,

The customer is having a situation running the processor M3 of the card F28M36 with CCS.

This is the Error message:
Cortex_M3_0: SemiHosting : Read Failure : Memory at Address: 3ff00000 Length: c

This problem occurs only with the M3 processor, not with the C28 processor
This error message appears after clicking on resume.

Do you have any possible solution for this?

Thanks,

Jonathan