Part Number: MSP430FG6626
Tool/software: Code Composer Studio
Hi,
I’m working with the MSP430FG6626 and have a question concerning the CTSD16 and the visibility of registers in debugging mode, respectively:
When I’m debugging I can only view registers of Channel 0 in the register tab, e.g. CTSD16CCTL0.
How can I make the registers of the other AD-channels visible, e.g. CTSD16CCTL1?
As an IDE I’m using CCS 10.1.0.
The example project I’m debugging is msp430fg662x_ctsd16_04 and I try to use channel 1 instead of channel 0.
Thank you very much.