Part Number: LAUNCHCC3220MODASF
Other Parts Discussed in Thread: CC3220SF
Tool/software: Code Composer Studio
Hello Ti team
I am working on CC3220MODASF SDK. I have successfully built the example project in workspace folder and I have added this workspace folder in git using following commands:
// Initialize git
git init
// Add workspace folder in git
got add <workspace folder>
// Git commit
Git commit -m <commit message>
// git push
git push origin <branch name>
After following above git steps workspace folder uploaded successfully. For cross verification of uploaded code I am cloning the code from my GitHub in same location and I am getting following compilation error:
error #10008-D: cannot find file "freertos_builds_CC3220SF_LAUNCHXL_release_ccs.lib
I also followed this link too and got same results as above attached screenshot.
I also tried git tag to release the workspace but same issue.
Anyone help to resolve the issue so that I can push the code to GitHub and clone/pull the code and it can compile successfully so that each time when I will change the code I do not have to release by creating zip file and upload via Dropbox/gdrive.
Any help will be appreciate.
Thanks.