Other Parts Discussed in Thread: MMWAVEICBOOST
Tool/software: Code Composer Studio
Hello,
I'd like to deal with the ccs project with AWR6843ISK at debug mode.
After project is compiled, the emulator can not be connected to the EVK.
Test Environment, a figure of EVK Setup, Test Connection Log and figure of BH XDS560v2 configuration utility & log is listed below.
Please assist.
<Test Environment>
EVK : AWR6843ISK + MMWAVEICBOOST
CCS version : 10.1.1.00004
SDK version : mmwave_sdk_03_04_00_03
Emulator : BH XDS560v2-USB System Trace Emulator
CCS Project Name : 68xx_mmwave_sdk_hwa (mmwave_automotive_toolbox_3_1_0\mmwave_sdk_ccs_projects\mmwave_sdk_3_4)
<EVK Setup>
< Test Connection Log >
[Start: Blackhawk XDS560v2-USB System Trace Emulator_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\Soo\AppData\Local\TEXASI~1\CCS\
ccs1011\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'bh560v2u.out'.
Loaded FPGA Image: C:\ti\ccs1011\ccs\ccs_base\common\uscif\dtc_top.jbc
The library build date was 'May 7 2020'.
The library build time was '19:55:51'.
The library package version is '9.2.0.00002'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '6' (0x00000006).
The controller has an insertion length of '0' (0x00000000).
The cable+pod has a version number of '8' (0x00000008).
The cable+pod has a capability number of '7423' (0x00001cff).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the Nano-TBC VHDL.
The link is a 560-class second-generation-560 cable.
The software is configured for Nano-TBC VHDL features.
The controller will be software reset via its registers.
The controller has a logic ONE on its EMU[0] input pin.
The controller has a logic ONE on its EMU[1] input pin.
The controller will use falling-edge timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '2' (0x0002).
The utility logic has not previously detected a power-loss.
The utility logic is not currently detecting a power-loss.
Loaded FPGA Image: C:\ti\ccs1011\ccs\ccs_base\common\uscif\dtc_top.jbc
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.
The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
[End: Blackhawk XDS560v2-USB System Trace Emulator_0]
<BH XDS560v2 configuration utility>
< Output log of Configuration Utility >
CMD: dtc_conf --version
Version 9.2.0.00002, built May 7 2020 21:04:33
LAN: Not selected to search.
CMD: dtc_conf get bh560v2u 0
CMD: dtc_conf get bh560v2u 1
USB: 1 device found.
TOTAL: 1 device found.
CMD: dtc_conf get bh560v2u 0
addrConf=:55756
addrIo=:55755
boardRev=2
dtcName=none
epkRev=5.0.573.0
fpgaRev=1.57
productClass=XDS560V2
productName=Blackhawk USB560v2 System Trace Emulator
safeMode=false
serialNum=00:00:00:04:55:49
swBuildTime=Apr 19 2012 14:09:25
swRev=5.0.573.0
time=none
vendorName=Blackhawk
standbyEnable=false
standbyMinutes=20
CMD: dbgjtag -X emulator,driver=bh560v2u,ioport=0 -S integrity -Y reset -S pathlength -G range,lowest=9.350000,highest=11.250000
Loaded FPGA Image: C:\ti\ccs1011\ccs\ccs_base\common\uscif\dtc_top.jbc
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.
The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
RES: dbgjtag -X emulator,driver=bh560v2u,ioport=0 -S integrity -Y reset -S pathlength -G range,lowest=9.350000,highest=11.250000
RES: Fail