Part Number: TMS570LS3137
Other Parts Discussed in Thread: TMS570LS1224, HALCOGEN
Tool/software: Code Composer Studio
Hello,
I have made my own board with TMS570LS1224 micro-controller and I program the code with XDS100-v2 emulator.
When I click run and debug button in ccs, I get this error:
I made these changes: In debug mode of ccs when running the code went to Tools->On Chip Flash and selected "Entire Flash" checkbox. Then I clicked the very bottom "Erase Flash" button. Also I checked Tools->ARM Advanced Features weather the enabled checkbox is enabled.
But when I reprogram the board, nothing changed as below:
And this is disassembly if helps:
Can someone help please?