Part Number: TIDM-THDREADING
Tool/software: Code Composer Studio
The power meter software “EnergyLibraryi2040TTwoPhaseConfiguration-3.1” works perfect when tested in our lab across the load.
The added feature for THD software “TIDMTHDREADING-1.0” is the one that doesn’t work properly (only works with no load), as soon as load is applied the RMS voltage and THVD readings from the TI board goes to zero.
It seems the sampling rate is the same for both software, so my guess is that parameters built within the TI board to measure harmonics has something to do with that.
The simulation I did has a high harmonic content (between 60%-600% THVD). Is there any limitation on the software for THD measurements? What is the higher order harmonic content the board is design to handle?
We need help ASAP.