This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/PROCESSOR-SDK-AM335X: SYS/BIOS v6.46.5.55 is not currently installed - BUT IT IS!

Part Number: PROCESSOR-SDK-AM335X

Tool/software: Code Composer Studio

Hello.

Screwed over by CCS yet again.  (Not to be confused with the forum screwing my over by telling me I can't post with my old email address, and WILL NOT LET ME UPDATE IT!)

Giving into the pressure of upgrading to version 10, from version 7.2, because of the excessive constant crashes of 7.2, it told me that it had to update the workspace in a manner that would make it incompatible with previous versions.

Then I try to build a small test project,  and it commences to tell me my products are not there.

Well, you know what??  It is there.  Right in front of my face.  And I've been using it for a few years.

So... now my workspace has been screwed with fouling up CCS7, and my new projects won't build because this thing doesn't understand 'leading zeros'.

Any wonder I have such distain for this environment??  Did no one test this for regression?   So insure it would function??

  • Hi Chris,

    Please check to see if CCS has "discovered" the SYS/BIOS installation. You can check in the workspace preference:

    If it does not appear in the "Discovered products" list, then press the "Refresh" button on the right to have CCS search for products to "discover". It will look in all the directories in the "Product discover path" list.

    Thanks

    ki

  • Got it. Thanks.

    It also set it to the wrong XDC tools, and was counter-intuitive on how to set it to the right one.

    CCS 7 clearly has a drop down for XDC.  This, you have to double click on it and tell it to stop setting it to things I don't want.