This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP432P401R: Error connecting to the target: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 8.4.0.00006)

Part Number: MSP432P401R

Tool/software: Code Composer Studio

I was doing a project and was working with 5V and im not sure if i connected something wrong, but when i plugged it in it seemed fine but when i tried to flash code onto the msp432 it gave me that error
 Error connecting to the target: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 8.4.0.00006)