Part Number: CC2652R
Other Parts Discussed in Thread: SYSCONFIG
Tool/software: Code Composer Studio
Hi, TI expert
The customer has an inquiry regarding the control of the RF output of the CC2652R1 module.
For RF control, SmartRF Studio7 refers to the TxPower register value table corresponding to each output as shown in the figure below, and at the code level, the table automatically created by the SYSCONFIG program is being used.
However, it is not possible to control the level for the middle value of the table such as specific TxPower (-1, -2, -4, -7, -8, -11, -13, -14, -16, -17, -19).
[Questions]
1) Is it possible to arbitrarily change the TxPower register value and control it with the Tx Power not indicated in the output table?
2) Can I check the register value corresponding to the above specific TxPower (-1, -2, -4, -7, -8, -11, -13, -14, -16, -17, -19)?
Please answer me.
Thank you.