Part Number: MSP430FR2355
Tool/software: TI C/C++ Compiler
I have a 2355 Development board that works fine but lately when I right click on my project and build. It builds then 'sometimes' downloads but then errors out with the following messages. Nothing has changed from a hardware standpoint. I have touched things in the properties settings of CCS over time (not sure what anymore). Can someone tell me what is going on. If I click the stop button and then the 'bug icon' at the top which builds and reloads all seems to load again without error?????
MSP430: Flash/FRAM usage is 1424 bytes. RAM usage is 186 bytes.
MSP430: Trouble Writing Memory Block at 0x8000 on Page 0 of Length 0x54e: Could not erase device memory
MSP430: File Loader: Verification failed: Target failed to write 0x08000
MSP430: GEL: File: D:\Customers\Firmware\MSP2355_Sandbox\Debug\MSP2355_Sandbox.out: Load failed.