This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler: What compiler (in Win10) is suggested to develop SMPS by using MCU UCD3138?

Other Parts Discussed in Thread: UCD3138

Tool/software: TI C/C++ Compiler

What ARM compiler (in Win10) is suggested to develop SMPS by using MCU UCD3138?

5.2.4 ?

5.2.9 ?

or others?

  • Hi,

    Many UCD3138 EVM firmware were developed by compiler version 5.2.4.

    So if you use 5.2.9, you will be fine, but may need to tweak some settings.

    For example, CCS may forget the 32-bit/ARM code option setting of some files if you switch to a different version of compiler.

    Which can be easily reconfigured in the project setting, but with 5.2.4 you will not even need to do that.

    Regards,