This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC3220SF: CC3220SF

Part Number: CC3220SF

Tool/software: Code Composer Studio

Is CCS already supported for macOS Big Sur?  If not, is there an ETA?

  • Hello,

    It is not currently supported. There is no current ETA though it will not be until sometime early next year at the earliest.

    Thanks

    ki 

  • Thanks for the update Ki, sad it will take such a long time - I realize that many do not work on a Mac so probably not a priority to TI.

    In the meantime, I have CCS 10 loaded on Big Sur running in a VM. Install went fine and compilation seems to do ok also. I cannot connect to a LAUNCH pad target but that can be as much a problem of the VM as Big Sur. I may create a VM with Catalina on it see if that goes with CCS 10 and keep that around in case it does. I will need to start updating my Macs to Big Sur as they are used for other dev projects (involving Xcode).