Other Parts Discussed in Thread: OMAPL138
Tool/software: Code Composer Studio
Hello
I got the following error while linking the available USB driver for OMAPL138 development board lcdkOmapl138.
=============================================================
.."../OMAPL138.cmd", line 55: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. run placement with alignment fails for section ".bss" size 0x9650c. Available memory ranges:
SHRAM size: 0x20000 unused: 0xf538 max hole: 0xf538
======================================================================================================
I have added my .cmd file for the project,Please let me help to resolve the issue.i have done the optimization also for the project but error remains same.
i have attached my .cmd file for the project,Please let me help to resolve the issue.
====================================================================================
/****************************************************************************/
/* OMAPL138.cmd */
/* Copyright (c) 2010 Texas Instruments Incorporated */
/* Author: Rafael de Souza */
/* */
/* Description: This file is a sample linker command file that can be */
/* used for linking programs built with the C compiler and */
/* running the resulting .out file on an OMAPL138 */
/* device. Use it as a guideline. You will want to */
/* change the memory layout to match your specific */
/* target system. You may want to change the allocation */
/* scheme according to the size of your program. */
/* */
/* Usage: The map below contains the local memory for each core */
/* Use the linker option --define=DSP_CORE=n */
/* Where n defines the core used: DSP (n=1) or ARM (n=0) */
/* */
/****************************************************************************/
MEMORY
{
#ifdef DSP_CORE /* DSP exclusive memory regions */
DSPL2ROM o = 0x00700000 l = 0x00100000 /* 1MB L2 DSP local ROM */
DSPL2RAM o = 0x00800000 l = 0x00040000 /* 256kB L2 DSP local RAM */
DSPL1PRAM o = 0x00E00000 l = 0x00008000 /* 32kB L1 DSP local Program RAM */
DSPL1DRAM o = 0x00F00000 l = 0x00008000 /* 32kB L1 DSP local Data RAM */
#endif
SHDSPL2ROM o = 0x11700000 l = 0x00100000 /* 1MB L2 Shared Internal ROM */
SHDSPL2RAM o = 0x11800000 l = 0x00040000 /* 256kB L2 Shared Internal RAM */
SHDSPL1PRAM o = 0x11E00000 l = 0x00008000 /* 32kB L1 Shared Internal Program RAM */
SHDSPL1DRAM o = 0x11F00000 l = 0x00008000 /* 32kB L1 Shared Internal Data RAM */
EMIFACS0 o = 0x40000000 l = 0x20000000 /* 512MB SDRAM Data (CS0) */
EMIFACS2 o = 0x60000000 l = 0x02000000 /* 32MB Async Data (CS2) */
EMIFACS3 o = 0x62000000 l = 0x02000000 /* 32MB Async Data (CS3) */
EMIFACS4 o = 0x64000000 l = 0x02000000 /* 32MB Async Data (CS4) */
EMIFACS5 o = 0x66000000 l = 0x02000000 /* 32MB Async Data (CS5) */
SHRAM o = 0x80000000 l = 0x00020000 /* 128kB Shared RAM */
DDR2 o = 0xC0000000 l = 0x20000000 /* 512MB DDR2 Data */
#ifndef DSP_CORE /* ARM exclusive memory regions */
ARMROM o = 0xFFFD0000 l = 0x00010000 /* 64kB ARM local ROM */
ARMRAM o = 0xFFFF0000 l = 0x00002000 /* 8kB ARM local RAM */
#endif
}
SECTIONS
{
.text > SHRAM
.stack > SHRAM
.bss > SHRAM
.cio > SHRAM
.const > SHRAM
.data > SHRAM
.switch > SHRAM
.sysmem > SHRAM
.far > SHRAM
.args > SHRAM
.ppinfo > SHRAM
.ppdata > SHRAM
/* TI-ABI or COFF sections */
.pinit > SHRAM
.cinit > SHRAM
/* EABI sections */
.binit > SHRAM
.init_array > SHRAM
.neardata > SHRAM
.fardata > SHRAM
.rodata > SHRAM
.c6xabi.exidx > SHRAM
.c6xabi.extab > SHRAM
}
=========================================================================================================
Thanks in advance
regards
shubham