Part Number: CC2642R
Other Parts Discussed in Thread: SYSBIOS, SYSCONFIG
Tool/software: Code Composer Studio
Hi Teams,
1. Test condition:
Compile based on
Hardware: CC2642R1F
Software: CCS 9.0.1; SDK 4.30.00.54,
Project Import: C:\ti\simplelink_cc13x2_26x2_sdk_4_30_00_54\examples\rtos\CC26X2R1_LAUNCHXL\ble5stack\project_zero
2. Test Result:
making ../src/sysbios/rom_sysbios.aem4f ...
Building file: "../project_zero.syscfg"
Invoking: System Configuration Tool
"C:/ti/ccs901/ccs/tools/node/node.exe" "C:/ti/ccs901/ccs/utils/sysconfig/cli.js" -s "C:/ti/simplelink_cc13x2_26x2_sdk_4_30_00_54/.metadata/product.json" -o "syscfg" --compiler ccs "../project_zero.syscfg"
gmake[1]: Nothing to be done for 'all'.
Usage:
cli [-o <dir>] [-s <file>] [-u <string>] [-b <name>] [-d <name>] [-p <name>] [-r <name>] [--treatWarningsAsErrors] <script>
cli --help
cli --version
example: cli -s meta_data/sdk.json -d MSP432P401R scripts/two_uarts.js
example: -s sdk.json -d MSP432P401R -o ./display_cfg sdk/cfgs/display.syscfg
Note that the all arguments other than '--help' and '--version' may also be
specified via the script with an embedded @cliArgs comment directive.
E.g. // @cliArgs -d MSP432P401R
If an argument is embedded in a script and exliciltiy specified via the CLI
then precedence is given to the CLI arguments. Additionally, specifying
"--board" or "--device" on the CLI will override any "--board" and "--device"
arguments specified in the script.
subdir_rules.mk:12: recipe for target 'build-1778024223-inproc' failed
Invalid argument '-s': C:\ti\simplelink_cc13x2_26x2_sdk_4_30_00_54\.metadata\product.json: Validation failed: [
{
"keyword": "additionalProperties",
"dataPath": "",
"schemaPath": "#/additionalProperties",
"params": {
"additionalProperty": "minToolVersion"
},
"message": "should NOT have additional properties"
}
]
gmake[1]: *** [build-1778024223-inproc] Error 1
gmake: *** [build-1778024223] Error 2
subdir_rules.mk:9: recipe for target 'build-1778024223' failed
gmake: Target 'all' not remade because of errors.
**** Build Finished ****
Regards,
Kevin