Part Number: CCSTUDIO
Other Parts Discussed in Thread: 66AK2H12
Tool/software: Code Composer Studio
Hi
When our customer run the program which I attached on this thread, the following fail message is asserted.
If they change the configuration for optimization to "not -O3" then the fail is not occurred.
Or if they compile the code on Visual Studio and not on CCS then the fail is not occurred.
Therefore, the fail may be caused from compiler.
- Device: 66AK2H12
- CCS #: CCS 10.1.1.00004 for Windows
For more information about the test, please refer to the attached test project.
Thanks and Best regards,
HaTa.