Part Number: TMDSLCDK138
Other Parts Discussed in Thread: OMAP-L138
Tool/software: Code Composer Studio
Hi,
We have a project where we are using the OMAP-L138.
Is it possible to load and run programs onto both the ARM9 and DSP at the same time for debugging?
Right now the only debug tool that is being used is the XDS100v3 over the JTAG port, and the DSP is running TI RTOS and the ARM9 were not sure if it is going to run the TI RTOS or Linux.
If this is possible, does TI have any documentation on being able to do this?
Thanks,
Ben