Part Number: TMS320F28335
Tool/software: Code Composer Studio
Hi,
Thanks in advance, Jorge.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28335
Tool/software: Code Composer Studio
Hi,
I would like to know a list of possible math operations in the workspace. (For example: sqrt())
Specifically, I need to link two Uint16 and read a Float
Thanks in advance, Jorge.
Thanks Keith Barkley
Sorry, I mean the math operations of global variables within Watch Windows.
Regards, Jorge.
Hello Ki,
I am working with Code Composer Studio 3.3 which requires an old project.
I add image for better understanding.
in the figure above:
View -> Watch Window
An example of a sum is shown in the image:
SUM_Ia_Ib: meas_grid.Ia + meas_grid.Ib
The sum works well.
But if I try sqrt(mas_grid.Ia) it doesn't work.
1)
I would like to know what are the possible functions that can be used within Watch Window.
2)
I need to read a float, which is composed of the union of two Uint16 (LOW and HIGH). Is it possible to perform this operation in the Watch Window? Could you help me?
Thank you very much in advance.
Best Regards, Jorge