Part Number: OMAP-L138
Other Parts Discussed in Thread: OMAPL138
Tool/software: TI C/C++ Compiler
Regards,
Friedrich
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Unfortunately, no. The C6000 Safety Compiler Qualification Kit only supports version 8.3.x.
Thanks and regards,
-George
Friedrich,
Have you set environment variable COVFILELIST according to the code coverage instructions in coverage_testing_instructions.pdf?
Look at the folder with instrumented binaries. You need to create a comma separate list of all the absolute paths to each *.cov file and set it to COVFILELIST
Regards,
Greg
Friedrich,
How did you swap out the instrumented binaries with the production compiler?
I would recommend using the approach from the coverage_testing_instructions.pdf
If you did above steps and are still getting the xdc build error for "cannot open source file", then please send more details on how you swapped out the instrumented binaries including your production compiler installation location.
If I remember correctly, there can be hidden errors in xdc builds that make debugging build issues more difficult. I believe a successful xdc build is required in order for the app_pe674.h file to be generated. So there may be some hidden build error.
Thanks
Greg
Looking back at your earlier post, I can see that it does appear that you have swapped out the instrumented binaries with the CCS production installation of 8.3.3.
....\tools\compiler\ti-cgt-c6000_8.3.3\bin\abs6x.cov
I'm assuming for your testing that you have the original binaries in
....\tools\compiler\ti-cgt-c6000_8.3.3\binold
and the instrumented binaries in
....\tools\compiler\ti-cgt-c6000_8.3.3\bincov
and that you are able to swap easily between the two by simply renaming binold to bin, or bincov to bin.
If you try building a simple CCS application (one that doesn't involve xdc) then does it build with no errors?
I'm guessing perhaps there are some unreported bullseye build errors that are causing the xdc build to "think" the build was a fail. So try with a non-xdc app to ensure there are no hidden bullseye errors indicating setup issues.
Thanks
Greg
Friedrich,
I'm getting some xdc experts involved so we can better understand the xdc errors as related to collecting coverage data.
Regards,
Greg
Hi Friedrich,
Which version of CCS, XDCtools and TI-RTOS are you using? To check the version of XDCtools used for the project build, go into Project Properties > General > Products. Please also share which TI software package you are using, if any.
Please make sure you have the correct search path for the missing file, both under Compiler options (Project Properties > Build > Compiler > Include Options) and under XDCtools options (Project Properties > Build > XDCtools > Basic Options).
You may also be missing a symbol definition such as "SOC_OMAPL138", "lcdkOMAPL138", or "omapl138" in your project settings.
If the error still persists after above, please post your full CCS build log so we can take a closer look. If you are able to zip up your project and post it here that would help as well.
Regards,
Sahin
Friedrich,
Does your xdc project build clean if you use the production compiler instead of the bullseye-instrumented binaries?
I'm suspecting that there's an issue while using bullseye coverage with xdc builds.
Unfortunately I'm not familiar with c6000 projects using xdc.
Could you please send details on how I can create a project similar to yours so I can try enabling bullseye and reproduce what you are seeing?
Thanks
Greg
Friedrich,
Thanks for confirming the issue only occurs with the bullseye coverage instrumented compiler.
Please send me details on how to create a project similar to yours so I can reproduce the issue.
Thanks
Greg
Friedrich,
I was able to build your project and I'm getting below error. xdc's environment is not working with bullseye.
From below you can see that the compiler version check is expecting cl6x.exe to return 8.3.3, however, some bullseye error is confusing it.
Building file: "../app.cfg"
Invoking: XDCtools
"C:/ti/ccs/ccs10.0.0/xdctools_3_61_00_16_core/xs" --xdcpath="C:/ti/bios_6_82_00_16/packages;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C674 -p ti.platforms.evm6748 -r release -c "C:/ti/compilers/ti-cgt-c6000_8.3.3" --compileOptions "-g" "../app.cfg"
making package.mak (because of package.bld) ...
ti.targets.elf.C674: warning: version match failed on 'BullseyeCoverage 8.16.1 error 8: atexit failed, errno=5 "Access is denied. "
8.3.3
'
I'm going to follow up with our xdc experts.
Regards,
Greg
Friedrich,
Sorry for the delays in helping you resolve this issue.
Where are you in your overall project development as related to applying the QKIT?
Is collecting code coverage the only remaining step?
What safety standard are you qualifying your project for? ASIL-B or ASIL-D?
Thanks
Greg
Friedrich,
In your overall safety qualification activity, what is your timeline for getting this coverage compare step done?
It looks like the main xdc expert we need to work with is out this week.
I've definitely confirmed that the xdc/xs build is not "seeing" the CCS project's environment variable setting for COVFILELIST. I can also see from xdc auto-generated files that it has a method for setting other environment variables. However, I'm not familiar enough with xdc configuration to determine a way to set additional environment variables.
Apologies again for taking so long with this.
Regards,
Greg
Thanks Friedrich. I'll get back to you early next week once our xdc expert is back.
Friedrich,
Please try below and let me know if you have any issues.
Set COVFILELIST in your CCS project in project-properties (same as mentioned in coverage user guide):
CCS BUILD -> Environment tab
Build your project which should fail.
Edit file: project_folder/Debug/configPkg/package/package.bld.xml
Change below:
rawVersion="8.3.3BullseyeCoverage 8.16.1 error 15: Cannot find C:\Users\a0196512\workspace_v10\c674_round10\Debug\configPkg/test.cov, errno=2 "The system cannot find the file specified. ". COVFILE is not set
To instead be this:
rawVersion="8.3.3"
Build again in CCS (but do not choose clean or rebuild)
The second build should not regenerate above xml or any already auto-generated makefiles.
Confirm that you have no bullseye errors in the console output, and confirm that all the *.cov file time stamps update.
Thanks
Greg
Friedrich,
Is there any other CCS project I can build to reproduce what you are seeing?
Any way to generate a cutdown test case and then send privately to me?
Thanks
Greg
Friedrich,
Apologies again for this messy work around and thanks for sending your project files. I was able to reproduce your build fail.
With addition of the extra sys/bios “features” in your second project, there are now two files that need rawVersion updated.
Here’s the build sequence that worked for me:
rebuild
[Fatal Error] package.bld.xml:24:163: Element type "target" must be followed by either attribute specifications, ">" or "/>".
fix both files with garbage rawVersion
C:\Users\greg\workspace_v8\c60_typical\Debug\configPkg\package\cfg\app_pe674.cfg
C:\Users\greg\workspace_v8\c60_typical\Debug\configPkg\package\package.bld.xml
build (not rebuild and not clean/build)
"C:/ti/ccs/ccs810/xdctools_3_50_07_20_core/packages/xdc/cfg/global.h", line 39: fatal error #1965: cannot open source file
"C:/Users/greg/workspace_v8/c60_typical/Debug/configPkg/package/cfg/app_pe674.h"
... then it does
configuring app.xe674 from package/cfg/app_pe674.cfg ...
build (not rebuild and not clean/build)
it works...
Once again apologies for the messy workaround. I'm submitting a bug against xdc for above issue.
Regards,
Greg