Part Number: LAUNCHXL2-RM46
Other Parts Discussed in Thread: RM46L852
Tool/software: Code Composer Studio
Hi there,
I recently purchased LAUNCHXL2-RM46 and installed CCS Version: 10.1.1.00004.
I started CCS, and then, to confirm LAUNCHXL2-RM46 debugging, connected it to my PC with USB cable.
then, LED was blinking on the board. But I could not start debugging.
Does anyone help me?
There was no LAUNCHXL2-RM46 detection in CCS I expected, when I connected board to my PC (already CCS running).
So I tried to make configuration manually,
Window->Show view->Target configuration .... Connection and Device was selected in the window.
Connection : Texas Instruments USB XDS110 debug probe
Device : RM46L852
Then save configuration, pushed Test Connection, following coming up:
-------------------------------------------------------------------------------------------------------
[Start: Texas Instruments XDS110 USB Debug Probe_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\SMACH1~1\AppData\Local\TEXASI~1\
CCS\ccs1011\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'May 7 2020'.
The library build time was '21:10:18'.
The library package version is '9.2.0.00002'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-260' (0xfffffefc).
The title is 'SC_ERR_XDS110_OPEN'.
The explanation is:
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the XDS110SupportReadMe.pdf
file there for instructions.
[End: Texas Instruments XDS110 USB Debug Probe_0]
-------------------------------------------------------------------------------------------------------
I also tried to search a device with xdsdfu.
-------------------------------------------------------------------------------------------------------
c:\ti\ccs1011\ccs\ccs_base\common\uscif\xds110>xdsdfu -e
USB Device Firmware Upgrade Utility
Copyright (c) 2008-2019 Texas Instruments Incorporated. All rights reserved.
Scanning USB buses for supported XDS110 devices...
Found 0 devices.
-------------------------------------------------------------------------------------------------------
Thanks.
H. Yamai