Part Number: LAUNCHXL-CC1352P
Other Parts Discussed in Thread: CC1352P, SYSCONFIG, CC1352R
Tool/software: Code Composer Studio
Hi everyone, i need to migrate a code written for the CC1352R1 with Code Composer Studio v.8.3.0, so without sysconfig tool, to my new CC1352P (precisely LAUNCHXL-CC1352P-4), using Code Composer Studio v10.0.0 and sysconfig v1.6.0. My first trial was to simply change the variant in Properties->Resource->General->Project, build the project and flash it on my board; no errors are shown. But debugging is clear that the system is not working; in particoular the code is stuck in this while cycle
void CC1352R1_LAUNCHXL_initGeneral(void)
{
Power_init();
if (PIN_init(BoardGpioInitTable) != PIN_SUCCESS) {
/* Error with PIN_init */
while (1);
}
/* Perform board-specific initialization */
Board_initHook();
}
I know that i'm surely doing wrong things, but i dont' know how to solve it without rewriting all the code exploiting the sysconfig tool (i need for now to avoid it). Do you have any ideas?