Part Number: CC1352R
Other Parts Discussed in Thread: UNIFLASH,
Tool/software: Code Composer Studio
Hi,
I have created a custom board with the CC1352R IC. I was initially able to connect to the debugger and flash new programs in it. After flashing the rfWsnNode example, im unable to connect to the debugger. I have tried using smartRF flash programmer 2 and uniflash, but i cant force an entire flash erase. Both softwares are unable to connect to the device and throw out errors while attempting a forced erase. Im not able to connect to the DAP also on code composer studio. The hardware connections on the chip are fine because the currently loaded rfWsnNode example runs on it and the custom board is transmitting data.
Could you please advise what steps can I take to fix this.
Thank you,
Shitij