Part Number: MMWAVEICBOOST
Tool/software: Code Composer Studio
Hello,
I'm using the overhead_mount_occupancy demo. The user guide mentions that XDS110 firmware needs to downgrade to version 2.3.0.18.
It says if the XDS110 FW is not 2.3.0.18, the packet may lose. After I downgraded the FW, but the system would require to upgrade XDS110 FW to the latest version (I'm using CCS 10.1.1 ver.) when I used CCS debug. If I canceled the requirement of the upgrade information, I could not use CCS debug until I upgrade XDS110 FW.
Here are my questions,
1. Is the data obviously lose if we do not downgrade the XDS110 FW to version 2.3.0.18?
2. How can we continue to use CCS debug if we downgrade the XDS110 FW?
Best regrades,
Jack