Part Number: CC1312R
Other Parts Discussed in Thread: CC1310
Tool/software: Code Composer Studio
Dear Sir,
We implemented a subg coordinator(gateway) by CC1312R.
S/W SDK profile:
collector: based on 'ti154stack_linux_x64_4_30_00_06'
coprocessor: based on 'simplelink_cc13x2_26x2_sdk_4_30_00_54' coprocessor project
Issue:
Basically, it works well against sensors that are also implemented by CC1312R. (in long range mode)
But, yesterday, we used an Agilent spectrum to measure the RF transmit power of the collector module,
it shows only 2.6 dBm.
However, the option 'config-tx-power' in collector.cfg is set 14.
How can we debug this issue?
(PS)
1. The transmit power measured upon sensor side is 11 dBm which seems reasonable.
2. We also have a collector module implemented by CC1310. The measurement result
is normal. But, we run the same linux gateway software on both CC1312R1 collector module and
CC1310 collector module.
Thank you