This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Code Composer bug / C5515

CC version 4.2.1.00004

 

Hello,

Please find our CCS (version 4.2.1.00004) bug description:

 

If debug window is not shown on the screen when debugging beginning system crash.

If during debugging this windows was closed, system crash.

Please advise,

Best regards

Yaron

 

 

 

 

 

  • Yaron,

    I haven't seen CCS crash simply by closing the Debug view or having it closed when launching the debug session. There is one known issue where closing the Debug view while debugging causes an error dialog box to pop up on subsequent debug events. The error dialog box is titled "Multiple Errors have Occurred", and lists a number of "Asynchronous view update" error events. The workaround here is open the debug view and close and restart CCS.

    In general, it is advisable to keep the debug view open as without it most debug tasks like stepping and running cannot be performed. However, CCS should definitely not crash simply by closing the view. Could you provide additional crash logs as mentioned in this page: http://processors.wiki.ti.com/index.php/Troubleshooting_CCS#CCS_Diagnostic_Logs?