This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP-FET: Error Initializing Emulator: A firmware update is required for MSP430 Debug Interface

Part Number: MSP-FET

Tool/software: Code Composer Studio

When Running the Code Debug in CCS version 6 it works perfectly.

However, when we do the same in CCS version 9 it throws the following error.

I have not Updated this yet as i want to run the MSP-FET430UIF Debugger Interface on both platforms.

Will updating the firmware cause compatibility issues?

Moreover, how do i proceed with this issue?

Also How do I perform a roll back if this update causes some issues?