Part Number: TM4C1294NCPDT
Tool/software: Code Composer Studio
i am try to chip id read but unable to read chip id using spi so i needed solution in that how can read id i am mention my code
int main(void)
{
// uint32_t pui32DataRx[3];
ui32SysClkFreq = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480), 120000000);
ConfigureUART();
SSI0_int();
while(1)
{
PD_Reset();
Host_Command(HCMD_CLKEXT);
Host_Command(HCMD_ACTIVE);
SysCtlDelay(100);
// turn off screen output during startup
wr8(REG_GPIOX + RAM_REG, 0); // Set REG_GPIOX to 0 to turn off the LCD DISP signal
wr8(REG_PCLK + RAM_REG, 0); // Pixel Clock Output disable // load parameters of the physical screen to the Eve
// All of these registers are 32 bits, but most bits are reserved, so only write what is actually used
wr16(REG_HCYCLE + RAM_REG, HCYCLE); // Set H_Cycle to 548
wr16(REG_HOFFSET + RAM_REG, HOFFSET); // Set H_Offset to 43
wr16(REG_HSYNC0 + RAM_REG, HSYNC0); // Set H_SYNC_0 to 0
wr16(REG_HSYNC1 + RAM_REG, HSYNC1); // Set H_SYNC_1 to 41
wr16(REG_VCYCLE + RAM_REG, VCYCLE); // Set V_Cycle to 292
wr16(REG_VOFFSET + RAM_REG, VOFFSET); // Set V_OFFSET to 12
wr16(REG_VSYNC0 + RAM_REG, VSYNC0); // Set V_SYNC_0 to 0
wr16(REG_VSYNC1 + RAM_REG, VSYNC1); // Set V_SYNC_1 to 10
wr8(REG_SWIZZLE + RAM_REG, SWIZZLE); // Set SWIZZLE to 0
wr8(REG_PCLK_POL + RAM_REG, PCLK_POL); // Set PCLK_POL to 1
wr16(REG_HSIZE + RAM_REG, HSIZE); // Set H_SIZE to 480
wr16(REG_VSIZE + RAM_REG, VSIZE); // Set V_SIZE to 272
wr8(REG_CSPREAD + RAM_REG, CSPREAD); // Set CSPREAD to 1 (32 bit register - write only 8 bits)
wr8(REG_DITHER + RAM_REG, DITHER); // Set DITHER to 1 (32 bit register - write only 8 bits)
}
}
void SSI0_int(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
GPIOPinTypeGPIOOutput(GPIO_PORTD_BASE, GPIO_PIN_0);
GPIOPinTypeGPIOOutput(GPIO_PORTA_BASE, GPIO_PIN_3);
GPIOPadConfigSet(GPIO_PORTA_BASE, GPIO_PIN_3, GPIO_STRENGTH_2MA,GPIO_PIN_TYPE_STD); // Make default state as Pull- up.
GPIOPinConfigure(GPIO_PA2_SSI0CLK);
GPIOPinConfigure(GPIO_PA4_SSI0XDAT0);
GPIOPinTypeSSI(GPIO_PORTA_BASE,GPIO_PIN_4|GPIO_PIN_2);
SSIConfigSetExpClk(SSI0_BASE, ui32SysClkFreq, SSI_FRF_MOTO_MODE_1, SSI_MODE_MASTER, 1000000, 8);
SSIEnable(SSI0_BASE);
}
void Host_Command(uint8_t HCMD)
{
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3,0x00);
SSIDataPut(SSI0_BASE, HCMD);
SSIDataPut(SSI0_BASE, 0X00);// This second byte is set to 0 but if there is need for fancy, never used setups, then rewrite.
SSIDataPut(SSI0_BASE, 0X00);
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3,GPIO_PIN_3);
}
void PD_Reset(void)
{
GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_0,0x00);
SysCtlDelay(ui32SysClkFreq/300);
GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_0,GPIO_PIN_0);
SysCtlDelay(ui32SysClkFreq/500);
}
void wr32(uint32_t address, uint32_t parameter)
{
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, 0);
SSIDataPut(SSI0_BASE,(uint8_t)((address >> 16) | 0x80)); // RAM_REG = 0x302000 and high bit is set - result always 0xB0
SSIDataPut(SSI0_BASE,(uint8_t)(address >> 8)); // Next byte of the register address
SSIDataPut(SSI0_BASE,(uint8_t)address); // Low byte of register address - usually just the 1 byte offset
while(SSIBusy(SSI0_BASE)){}
SSIDataPut(SSI0_BASE,(uint8_t)(parameter & 0xff)); // Little endian (yes, it is most significant bit first and least significant byte first)
SSIDataPut(SSI0_BASE,(uint8_t)((parameter >> 8) & 0xff));
SSIDataPut(SSI0_BASE,(uint8_t)((parameter >> 16) & 0xff));
SSIDataPut(SSI0_BASE,(uint8_t)((parameter >> 24) & 0xff));
while(SSIBusy(SSI0_BASE)){}
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, GPIO_PIN_3);
}
void wr16(uint32_t address, uint16_t parameter)
{
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, 0);
SSIDataPut(SSI0_BASE,(uint8_t)((address >> 16) | 0x80)); // RAM_REG = 0x302000 and high bit is set - result always 0xB0
SSIDataPut(SSI0_BASE,(uint8_t)(address >> 8)); // Next byte of the register address
SSIDataPut(SSI0_BASE,(uint8_t)address); // Low byte of register address - usually just the 1 byte offset
while(SSIBusy(SSI0_BASE)){}
SSIDataPut(SSI0_BASE,(uint8_t)(parameter & 0xff)); // Little endian (yes, it is most significant bit first and least significant byte first)
SSIDataPut(SSI0_BASE,(uint8_t)(parameter >> 8));
while(SSIBusy(SSI0_BASE)){}
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, GPIO_PIN_3);
}
void wr8(uint32_t address, uint8_t parameter)
{
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, 0);
SSIDataPut(SSI0_BASE,(uint8_t)((address >> 16) | 0x80)); // RAM_REG = 0x302000 and high bit is set - result always 0xB0
SSIDataPut(SSI0_BASE,(uint8_t)(address >> 8)); // Next byte of the register address
SSIDataPut(SSI0_BASE,(uint8_t)(address)); // Low byte of register address - usually just the 1 byte offset
while(SSIBusy(SSI0_BASE)){}
SSIDataPut(SSI0_BASE,parameter);
while(SSIBusy(SSI0_BASE)){}
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, GPIO_PIN_3);
}
uint32_t rd32(uint32_t address)
{
uint32_t Data32;
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, 0);
SSIDataPut(SSI0_BASE,(address >> 16) & 0x3F);
SSIDataPut(SSI0_BASE,(address >> 8) & 0xff);
SSIDataPut(SSI0_BASE,address & 0xff);
SSIDataGet(SSI0_BASE, &pui32DataRx[ui32Index]);
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, GPIO_PIN_3);
Data32 = + ((uint32_t)pui32DataRx[1] << 8) + ((uint32_t)pui32DataRx[2] << 16) + ((uint32_t)pui32DataRx[3] << 24);
return (Data32);
}
uint16_t rd16(uint32_t address)
{
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, 0);
SSIDataPut(SSI0_BASE,(address >> 16) & 0x3F);
SSIDataPut(SSI0_BASE,(address >> 8) & 0xff);
SSIDataPut(SSI0_BASE,address & 0xff);
SSIDataGet(SSI0_BASE, &pui32DataRx[ui32Index]);
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, GPIO_PIN_3);
uint16_t Data16 = pui32DataRx[0] + ((uint16_t)pui32DataRx[1] << 8);
return (Data16);
}
uint8_t rd8(uint32_t address)
{
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, 0);
SSIDataPut(SSI0_BASE,(address >> 16) & 0x3F);
SSIDataPut(SSI0_BASE,(address >> 8) & 0xff);
SSIDataPut(SSI0_BASE,address & 0xff);
SSIDataGet(SSI0_BASE, &pui32DataRx[ui32Index]);
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, GPIO_PIN_3);
return (pui32DataRx[0]);
}
// Read the specific ID register and return TRUE if it is the expected 0x7C otherwise.
uint8_t Cmd_READ_REG_ID(void)
{
uint32_t pui32DataRx[2];
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, 0);
SSIDataPut(SSI0_BASE,0x30); // Base address RAM_REG = 0x302000
SSIDataPut(SSI0_BASE,0x20);
SSIDataPut(SSI0_BASE,REG_ID); // REG_ID offset = 0x00
SSIDataPut(SSI0_BASE,0x00);
SSIDataGet(SSI0_BASE, &pui32DataRx[ui32Index]); // There was a dummy read of the first byte in there
SSIDataPut(SSI0_BASE,0x00);
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, GPIO_PIN_3);
if (pui32DataRx[0] == 0x7C) // FT81x Datasheet section 5.1, Table 5-2. Return value always 0x7C
{
return 1;
}
else
{
return 0;
}
}
//////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////hedder file ------------------> ft812.h
/*
* FT812.h
*
* Created on: Dec 20, 2020
* Author: gk
*/
#ifndef FT812_H_
#define FT812_H_
// =====================================================================================
// Required Functions - Hardware driver or otherwise environment specific. Abstracted |
// and found in ArduinoAL.h or whatever the abstraction layer is called in your world. |
// This library requires base support functions for SPI, delays, and hardware pin |
// control. |
// =====================================================================================
#undef DISPLAY
// Once again, if this is being used for Arduino, it wants C++, but C is totally cool as long as it is
// wrapped in this extern declaration (also see the bottom of the file for the close bracket)
#ifdef __cplusplus
extern "C" {
#endif
#define HCMD_ACTIVE 0x00
#define HCMD_STANDBY 0x41
#define HCMD_SLEEP 0x42
#define HCMD_PWRDOWN 0x50
#define HCMD_CLKINT 0x48
#define HCMD_CLKEXT 0x44
#define HCMD_CLK48M 0x62
#define HCMD_CLK36M 0x61
#define HCMD_CORERESET 0x68
#define CMD_APPEND 0xFFFFFF1E
#define CMD_BGCOLOR 0xFFFFFF09
#define CMD_BUTTON 0xFFFFFF0D
#define CMD_CALIBRATE 0xFFFFFF15 // 4294967061UL
#define CMD_CLOCK 0xFFFFFF14
#define CMD_COLDSTART 0xFFFFFF32
#define CMD_CRC 0xFFFFFF18
#define CMD_DIAL 0xFFFFFF2D
#define CMD_DLSTART 0xFFFFFF00
#define CMD_FGCOLOR 0xFFFFFF0A
#define CMD_GAUGE 0xFFFFFF13
#define CMD_GETMATRIX 0xFFFFFF33
#define CMD_GETPROPS 0xFFFFFF25
#define CMD_GETPTR 0xFFFFFF23
#define CMD_GRADCOLOR 0xFFFFFF34
#define CMD_GRADIENT 0xFFFFFF0B
#define CMD_INFLATE 0xFFFFFF22
#define CMD_INTERRUPT 0xFFFFFF02
#define CMD_KEYS 0xFFFFFF0E
#define CMD_LOADIDENTITY 0xFFFFFF26
#define CMD_LOADIMAGE 0xFFFFFF24
#define CMD_LOGO 0xFFFFFF31
#define CMD_MEDIAFIFO 0xFFFFFF39
#define CMD_MEMCPY 0xFFFFFF1D
#define CMD_MEMCRC 0xFFFFFF18
#define CMD_MEMSET 0xFFFFFF1B
#define CMD_MEMWRITE 0xFFFFFF1A
#define CMD_MEMZERO 0xFFFFFF1C
#define CMD_NUMBER 0xFFFFFF38
#define CMD_PLAYVIDEO 0xFFFFFF3A
#define CMD_PROGRESS 0xFFFFFF0F
#define CMD_REGREAD 0xFFFFFF19
#define CMD_ROTATE 0xFFFFFF29
#define CMD_SCALE 0xFFFFFF28
#define CMD_SCREENSAVER 0xFFFFFF2F
#define CMD_SCROLLBAR 0xFFFFFF11
#define CMD_SETBITMAP 0xFFFFFF43
#define CMD_SETFONT 0xFFFFFF2B
#define CMD_SETMATRIX 0xFFFFFF2A
#define CMD_SKETCH 0xFFFFFF30
#define CMD_SLIDER 0xFFFFFF10
#define CMD_SNAPSHOT 0xFFFFFF1F
#define CMD_SPINNER 0xFFFFFF16
#define CMD_STOP 0xFFFFFF17
#define CMD_SWAP 0xFFFFFF01
#define CMD_TEXT 0xFFFFFF0C
#define CMD_TOGGLE 0xFFFFFF12
#define CMD_TRACK 0xFFFFFF2C
#define CMD_TRANSLATE 0xFFFFFF27
#define CMD_VIDEOFRAME 0xFFFFFF41
#define CMD_VIDEOSTART 0xFFFFFF40
#define DLSWAP_FRAME 2UL
#define OPT_CENTER 1536UL
#define OPT_CENTERX 512UL
#define OPT_CENTERY 1024UL
#define OPT_FLAT 256UL
#define OPT_MONO 1UL
#define OPT_NOBACK 4096UL
#define OPT_NODL 2UL
#define OPT_NOHANDS 49152UL
#define OPT_NOHM 16384UL
#define OPT_NOPOINTER 16384UL
#define OPT_NOSECS 32768UL
#define OPT_NOTICKS 8192UL
#define OPT_RIGHTX 2048UL
#define OPT_SIGNED 256UL
// Definitions for FT8xx co processor command buffer
#define FT_DL_SIZE (8*1024) // 8KB Display List buffer size
#define FT_CMD_FIFO_SIZE (4*1024) // 4KB coprocessor Fifo size
#define FT_CMD_SIZE (4) // 4 byte per coprocessor command of EVE
// Memory block base addresses
#define RAM_G 0x0
#define RAM_DL 0x300000
#define RAM_REG 0x302000
#define RAM_CMD 0x308000
// Graphics Engine Registers - FT81x Series Programmers Guide Section 3.1
// Addresses defined as offsets from the base address called RAM_REG and located at 0x302000
// Discussion: Defining this way leads to an additional add operation in code that can be avoided by defining
// these addresses as 32 bit values, but this is easily paid for in clarity and coorelation to documentation.
// Further, you can add defines together in code and allow the precompiler to do the add operation (as here).
#define REG_CSPREAD 0x68
#define REG_DITHER 0x60
#define REG_DLSWAP 0x54
#define REG_HCYCLE 0x2C
#define REG_HOFFSET 0x30
#define REG_HSIZE 0x34
#define REG_HSYNC0 0x38
#define REG_HSYNC1 0x3C
#define REG_OUTBITS 0x5C
#define REG_PCLK 0x70
#define REG_PCLK_POL 0x6C
#define REG_PLAY 0x8C
#define REG_PLAYBACK_FORMAT 0xC4
#define REG_PLAYBACK_FREQ 0xC0
#define REG_PLAYBACK_LENGTH 0xB8
#define REG_PLAYBACK_LOOP 0xC8
#define REG_PLAYBACK_PLAY 0xCC
#define REG_PLAYBACK_READPTR 0xBC
#define REG_PLAYBACK_START 0xB4
#define REG_PWM_DUTY 0xD4
#define REG_ROTATE 0x58
#define REG_SOUND 0x88
#define REG_SWIZZLE 0x64
#define REG_TAG 0x7C
#define REG_TAG_X 0x74
#define REG_TAG_Y 0x78
#define REG_VCYCLE 0x40
#define REG_VOFFSET 0x44
#define REG_VOL_SOUND 0x84
#define REG_VOL_PB 0x80
#define REG_VSYNC0 0x4C
#define REG_VSYNC1 0x50
#define REG_VSIZE 0x48
// Touch Screen Engine Registers - FT81x Series Programmers Guide Section 3.3
// Addresses defined as offsets from the base address called RAM_REG and located at 0x302000
#define REG_TOUCH_CONFIG 0x168
#define REG_TOUCH_TRANSFORM_A 0x150
#define REG_TOUCH_TRANSFORM_B 0x154
#define REG_TOUCH_TRANSFORM_C 0x158
#define REG_TOUCH_TRANSFORM_D 0x15C
#define REG_TOUCH_TRANSFORM_E 0x160
#define REG_TOUCH_TRANSFORM_F 0x164
// Resistive Touch Engine Registers - FT81x Series Programmers Guide Section 3.3.3 - Document confused
// Addresses defined as offsets from the base address called RAM_REG and located at 0x302000
#define REG_TOUCH_ADC_MODE 0x108
#define REG_TOUCH_CHARGE 0x10C
#define REG_TOUCH_DIRECT_XY 0x18C
#define REG_TOUCH_DIRECT_Z1Z2 0x190
#define REG_TOUCH_MODE 0x104
#define REG_TOUCH_OVERSAMPLE 0x114
#define REG_TOUCH_RAW_XY 0x11C
#define REG_TOUCH_RZ 0x120
#define REG_TOUCH_RZTHRESH 0x118
#define REG_TOUCH_SCREEN_XY 0x124
#define REG_TOUCH_SETTLE 0x110
#define REG_TOUCH_TAG 0x12C
#define REG_TOUCH_TAG_XY 0x128
// Capacitive Touch Engine Registers - FT81x Series Programmers Guide Section 3.3.4
// Addresses defined as offsets from the base address called RAM_REG and located at 0x302000
#define REG_CTOUCH_MODE 0x104
#define REG_CTOUCH_EXTEND 0x108
#define REG_CTOUCH_RAW_XY 0x11C
#define REG_CTOUCH_TOUCH_XY 0x124
#define REG_CTOUCH_TOUCH1_XY 0x11C
#define REG_CTOUCH_TOUCH2_XY 0x18C
#define REG_CTOUCH_TOUCH3_XY 0x190
#define REG_CTOUCH_TOUCH4_X 0x16C
#define REG_CTOUCH_TOUCH4_Y 0x120
#define REG_CTOUCH_TAG 0x12C
#define REG_CTOUCH_TAG1 0x134
#define REG_CTOUCH_TAG2 0x13C
#define REG_CTOUCH_TAG3 0x144
#define REG_CTOUCH_TAG4 0x14C
#define REG_CTOUCH_TAG_XY 0x128
#define REG_CTOUCH_TAG1_XY 0x130
#define REG_CTOUCH_TAG2_XY 0x138
#define REG_CTOUCH_TAG3_XY 0x140
#define REG_CTOUCH_TAG4_XY 0x148
// Co-processor Engine Registers - FT81x Series Programmers Guide Section 3.4
// Addresses defined as offsets from the base address called RAM_REG and located at 0x302000
#define REG_CMD_DL 0x100
#define REG_CMD_READ 0xF8
#define REG_CMD_WRITE 0xFC
#define REG_CMDB_SPACE 0x574
#define REG_CMDB_WRITE 0x578
// Special Registers - FT81x Series Programmers Guide Section 3.5
// Addresses assumed to be defined as offsets from the base address called RAM_REG and located at 0x302000
#define REG_TRACKER 0x7000
#define REG_TRACKER_1 0x7004
#define REG_TRACKER_2 0x7008
#define REG_TRACKER_3 0x700C
#define REG_TRACKER_4 0x7010
#define REG_MEDIAFIFO_READ 0x7014
#define REG_MEDIAFIFO_WRITE 0x7018
// Miscellaneous Registers - FT81x Series Programmers Guide Section 3.6 - Document inspecific about base address
// Addresses assumed to be defined as offsets from the base address called RAM_REG and located at 0x302000
#define REG_CPU_RESET 0x20
#define REG_PWM_DUTY 0xD4
#define REG_PWM_HZ 0xD0
#define REG_INT_MASK 0xB0
#define REG_INT_EN 0xAC
#define REG_INT_FLAGS 0xA8
#define REG_GPIO 0x94
#define REG_GPIO_DIR 0x90
#define REG_GPIOX 0x9C
#define REG_GPIOX_DIR 0x98
#define REG_FREQUENCY 0x0C
#define REG_CLOCK 0x08
#define REG_FRAMES 0x04
#define REG_ID 0x00
#define REG_TRIM 0x10256C
#define REG_SPI_WIDTH 0x180
// Primitive Type Reference Definitions - FT81x Series Programmers Guide Section 4.5 - Table 6
#define BITMAPS 1
#define POINTS 2
#define LINES 3
#define LINE_STRIP 4
#define EDGE_STRIP_R 5
#define EDGE_STRIP_L 6
#define EDGE_STRIP_A 7
#define EDGE_STRIP_B 8
#define RECTS 9
// Bitmap Layout Format Definitions - FT81x Series Programmers Guide Section 4.7 - Table 7
#define ARGB1555 0
#define L1 1
#define L4 2
#define L8 3
#define RGB332 4
#define ARGB2 5
#define ARGB4 6
#define RGB565 7
#define TEXT8X8 9
#define TEXTVGA 10
#define BARGRAPH 11
#define PALETTED565 14
#define PALETTED4444 15
#define PALETTED8 16
#define L2 17
// Bitmap Parameters
#define REPEAT 1
#define BORDER 0
#define NEAREST 0
#define BILINEAR 1
// These defined "macros" are supplied by FTDI - Manufacture command bit-fields from parameters
// FT81x Series Programmers Guide is refered to as "FT-PG"
#define CLEAR(c,s,t) ((38UL<<24)|(((c)&1UL)<<2)|(((s)&1UL)<<1)|(((t)&1UL)<<0)) // CLEAR - FT-PG Section 4.21
#define CLEAR_COLOR_RGB(red,green,blue) ((2UL<<24)|(((red)&255UL)<<16)|(((green)&255UL)<<8)|(((blue)&255UL)<<0)) // CLEAR_COLOR_RGB - FT-PG Section 4.23
#define COLOR_RGB(red,green,blue) ((4UL<<24)|(((red)&255UL)<<16)|(((green)&255UL)<<8)|(((blue)&255UL)<<0)) // COLOR_RGB - FT-PG Section 4.28
#define VERTEX2II(x,y,handle,cell) ((2UL<<30)|(((x)&511UL)<<21)|(((y)&511UL)<<12)|(((handle)&31UL)<<7)|(((cell)&127UL)<<0)) // VERTEX2II - FT-PG Section 4.48
#define VERTEX2F(x,y) ((1UL<<30)|(((x)&32767UL)<<15)|(((y)&32767UL)<<0)) // VERTEX2F - FT-PG Section 4.47
#define CELL(cell) ((6UL<<24)|(((cell)&127UL)<<0)) // CELL - FT-PG Section 4.20
#define BITMAP_HANDLE(handle) ((5UL<<24) | (((handle) & 31UL) << 0)) // BITMAP_HANDLE - FT-PG Section 4.06
#define BITMAP_SOURCE(addr) ((1UL<<24)|(((addr)&1048575UL)<<0)) // BITMAP_SOURCE - FT-PG Section 4.11
#define BITMAP_LAYOUT(format,linestride,height) ((7UL<<24)|(((format)&31UL)<<19)|(((linestride)&1023UL)<<9)|(((height)&511UL)<<0)) // BITMAP_LAYOUT - FT-PG Section 4.07
#define BITMAP_SIZE(filter,wrapx,wrapy,width,height) ((8UL<<24)|(((filter)&1UL)<<20)|(((wrapx)&1UL)<<19)|(((wrapy)&1UL)<<18)|(((width)&511UL)<<9)|(((height)&511UL)<<0)) // BITMAP_SIZE - FT-PG Section 4.09
#define TAG(s) ((3UL<<24)|(((s)&255UL)<<0)) // TAG - FT-PG Section 4.43
#define POINT_SIZE(sighs) ((13UL<<24)|(((sighs)&8191UL)<<0)) // POINT_SIZE - FT-PG Section 4.36
#define BEGIN(PrimitiveTypeRef) ((31UL<<24)|(((PrimitiveTypeRef)&15UL)<<0)) // BEGIN - FT-PG Section 4.05
#define END() ((33UL<<24)) // END - FT-PG Section 4.30
#define DISPLAY() ((0UL<<24)) // DISPLAY - FT-PG Section 4.29
// Non FTDI Helper Macros
#define MAKE_COLOR(r,g,b) (( r << 16) | ( g << 8) | (b))
// Global Variables
extern uint16_t FifoWriteLocation;
// Function Prototypes
void PD_Reset(void);
void Host_Command(uint8_t HostCommand);
void wr32(uint32_t address, uint32_t parameter);
void wr16(uint32_t, uint16_t parameter);
void wr8(uint32_t, uint8_t parameter);
uint8_t rd8(uint32_t RegAddr);
uint16_t rd16(uint32_t RegAddr);
uint32_t rd32(uint32_t RegAddr);
void Send_CMD(uint32_t data);
void UpdateFIFO(void);
uint8_t Cmd_READ_REG_ID(void);
// Widgets and other significant screen objects
void Cmd_Slider(uint16_t x, uint16_t y, uint16_t w, uint16_t h, uint16_t options, uint16_t val, uint16_t range);
void Cmd_Spinner(uint16_t x, uint16_t y, uint16_t style, uint16_t scale);
void Cmd_Gauge(uint16_t x, uint16_t y, uint16_t r, uint16_t options, uint16_t major, uint16_t minor, uint16_t val, uint16_t range);
void Cmd_Dial(uint16_t x, uint16_t y, uint16_t r, uint16_t options, uint16_t val);
void Cmd_Track(uint16_t x, uint16_t y, uint16_t w, uint16_t h, uint16_t tag);
void Cmd_Number(uint16_t x, uint16_t y, uint16_t font, uint16_t options, uint32_t num);
void Cmd_Gradient(uint16_t x0, uint16_t y0, uint32_t rgb0, uint16_t x1, uint16_t y1, uint32_t rgb1);
void Cmd_Button(uint16_t x, uint16_t y, uint16_t w, uint16_t h, uint16_t font, uint16_t options, const char* str);
void Cmd_Text(uint16_t x, uint16_t y, uint16_t font, uint16_t options, const char* str);
void Cmd_SetBitmap(uint32_t addr, uint16_t fmt, uint16_t width, uint16_t height);
void Cmd_Memcpy(uint32_t dest, uint32_t src, uint32_t num);
void Cmd_GetPtr(void);
void Cmd_GradientColor(uint32_t c);
void Cmd_FGcolor(uint32_t c);
void Cmd_Translate(uint32_t tx, uint32_t ty);
void Cmd_Rotate(uint32_t a);
void Cmd_Scale(uint32_t sx, uint32_t sy);
void Cmd_Calibrate(uint32_t result);
uint16_t CoProFIFO_FreeSpace(void);
void Wait4CoProFIFO(uint32_t room);
void Wait4CoProFIFOEmpty(void);
void StartCoProTransfer(uint32_t address, uint8_t reading);
void CoProWrCmdBuf(const uint8_t *buffer, uint32_t count);
uint32_t WriteBlockRAM(uint32_t Add, const uint8_t *buff, uint32_t count);
// Panel specific setup parameters
//User selectable configurations.
#define EVE2_50
#ifdef EVE2_50
#define DWIDTH 800
#define DHEIGHT 480
#define PIXVOFFSET 0
#define PIXHOFFSET 0
#define HCYCLE 928
#define HOFFSET 88
#define HSYNC0 0
#define HSYNC1 48
#define VCYCLE 525
#define VOFFSET 32
#define VSYNC0 0
#define VSYNC1 3
#define PCLK 2
#define SWIZZLE 0
#define PCLK_POL 1
#define HSIZE 800
#define VSIZE 480
#define CSPREAD 0
#define DITHER 1
#endif
#ifdef __cplusplus
}
#endif
#endif /* FT812_H_ */