Part Number: DRA71XEVM
Tool/software: TI C/C++ Compiler
Hello,
I use 06.00.00.03 version SDK on 16.04 LTS of ubuntu.
When i executed ./setup.sh the "yocto-layers" and "config" folder were created outside of ti-processor-sdk-linux-automotive_dra7xx-evm_06_00_00_03 folder.
To execute ./bin/fetch-sources.sh, "yocto-layers" and "config" were needed to inside ti-processor-sdk-linux-automotive_dra7xx-evm_06_00_00_03, so copied them to this folder.
Then executed ./build-core-sdk.sh dra7xx-evm (Ofcourse, other steps before to this as per Developers guide followed).
After executing bitbake i am struggling with below errors, pls help me to fix them
ERROR: imglib-c66x-3_1_1_0-r1 do_install: Function failed: do_install (log file is located at /home/prasad.p/ti-processor-sdk-linux-automotive-dra7xx-evm-6.00.00.03/yocto-layers/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/imglib-c66x/3_1_1_0-r1/temp/log.do_install.12177)
ERROR: Logfile of failure stored in: /home/prasad.p/ti-processor-sdk-linux-automotive-dra7xx-evm-6.00.00.03/yocto-layers/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/imglib-c66x/3_1_1_0-r1/temp/log.do_install.12177
ERROR: Task (/home/prasad.p/ti-processor-sdk-linux-automotive-dra7xx-evm-6.00.00.03/yocto-layers/sources/meta-ti/recipes-ti/imglib/imglib-c66x_3.1.1.0.bb:do_install) failed with exit code '1'
ERROR: vlib-c66x-3_2_1_0-r0 do_install: Function failed: do_install (log file is located at /home/prasad.p/ti-processor-sdk-linux-automotive-dra7xx-evm-6.00.00.03/yocto-layers/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/vlib-c66x/3_2_1_0-r0/temp/log.do_install.12178)
ERROR: Logfile of failure stored in: /home/prasad.p/ti-processor-sdk-linux-automotive-dra7xx-evm-6.00.00.03/yocto-layers/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/vlib-c66x/3_2_1_0-r0/temp/log.do_install.12178
Pls find the attachments for the logs
PS: One thing what i noticed is the folder we get this related cp connot stat: No such file or directory, is empty. This could be the reason. But i do not know why this folder is empty.https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/81/Prasad.7z