Part Number: TMS320C6711D
Tool/software: Code Composer Studio
I'm using CCS 10.1.1.00004 and a Blackhawk XDS560v2 emulator. To debug this I've created the 'Hello world' example application. If I run Test Connection in the target configuration window I consistently get all the tests passing with no skips or failures. I have currently set TCLK to 5MHz though have also tried lower values. When I run debug I get 'Error connecting to the target: (Error -1060 @ 0x0)'. Interestingly if I enable the Debug Server Log in CCS support the hello world will then often start the debug session. However if I try this with my main application, even though the debug perspective may open, the debug commands (e.g. view memory) are unresponsive. Do you have any ideas or advice on what may be going wrong? I assume, as Test Connection consistently passes, I have a reliable JTAG connection but then why should this misbehave?
Any help much appreciated.