Part Number: LAUNCHXL-F280049C
Tool/software: Code Composer Studio
Back ground:
We have GPIO24, which is one of the default boot selection inputs, in use for SPI B which then interferes with the boot process.
I want to use just GPIO 32 select between Flash and SCI/Wait bootmodes.
I think I should do this by setting following
BOOTPIN_CONFIG = 0x5AFFFF20
BOOTDEF.BOOTDEF0 = 1 , wait SCI (when GPIO32 = 0, S2 on BOOSTXL on ie switch in the '0' position)
BOOTDEF.BOOTDEF1 = 3 , boot from Flash (when GPIO32 = 1, S2 on BOOSTXL off ie switch in the '1' position)
Is that correct?
What is the canonical way to program these OTP locations ( would prefer it that so that whenever
anyone pulls the project from GIT and just loads/runs the code in CCS the BOOTPIN and friends
will be set correctly as this will be our workflow for months to come.
Before programming the OTP locations I want to ensure everything is correct.
I think I should be able to emulate this by setting memory as follows:
0x0000 0D00: 5AFFFF20 FFFF0301 FFFFFFFF (copy pasted from the Memory Browser in 32 Bit Hex - TI Style)
Is this correct?
But how do I test this, exact steps would be great as although I've been through the One Day Workshop
for F280049 not everything clicked and matched what see in my CCS.
For example Reset Emulator is grayed out always. When I select Run/Reset/CPU nothing happens. Mostly I seem to be stuck at PC= 3FB02A