I have a fresh 64-bit Ubuntu 10.10 install on a laptop that I want to put my CCS companion license on.
So I downloaded CCSv5.0.2.00006.tar.gz
It took some work to get it to install. I had to install some 32-bit libraries just to get the install to happen.
I installed as root, and followed the instructions here... http://processors.wiki.ti.com/index.php/Linux_Host_Support#Installation_Instructions
Unfortunately, I can't get CCSv5 to launch. The launcher is on the desktop now. I double click, and no joy. I vi'd the launcher, and found the executable path at /usr/local/CCSv5/ccsv5/eclipse/eclipse. So I tried to run that from the command line, and no joy.
I ran an 'strace' on it, and saw myriad errors. 5468.output.txt
Any thoughts on what's keeping this from running? Thanks everybody!