Other Parts Discussed in Thread: EK-TM4C1294XL
I do have a EK-TM4C1294XL , but this is probably a general C code question, and if I enter that board, I am locked into posting on the board forum!?
I receive command strings by UDP. After handling a command, I return a string consisting of a number of elements stitched together in a new string.
Or in case of an unknown command or some conversion error, I return a Not Acknowleded (NAC).
I have somehow run into a problem. If the return string is too long, my return address on the stack is overwritten!
If the return strings are short enough, everything works for thousands of commands!
void ACK(char Cmd[], char Answ[])
{
char res[] = "0 ";
strcat(res, Cmd);
strcat(res, " ");
strcat(res, Answ); //If res string ends up too long, return address is overwritten!
udp_server_send(res);
}
void udp_incomming(void *arg, struct udp_pcb *pcb, struct pbuf *p, struct ip_addr *addr, u16_t port)
{
char Command[25];
char Catch[5], SweepParam[9];
char Answer[] = "----";
char b[10];
unsigned short c;
int a, i, j;
uint32_t Cardinal;
if (p != NULL) {
memcpy(Command,p->payload,p->len);
Command[p->len]=0;
memcpy(Catch,Command,4);
Catch[4]='\0';
ConvertError=false;
//Catch is a short string used to figure out which command I have received
---
if (ConvertError)
NAC(Command);
else
ACK(Command, Answer);
}
pbuf_free(p);
}
I am not all that well educated in C, but somehow I should clear more space on the stack, or maybe start using pointers.
But all that 'star'-stuff is still pretty alien to me!
How do I proceed?